SeamBuilderDefinitionMethods Enumeration¶
NXOpen.Features.ShipDesign.SeamBuilder.DefinitionMethods is an alias for NXOpen.Features.ShipDesign.SeamBuilderDefinitionMethods
-
class
NXOpen.Features.ShipDesign.
SeamBuilderDefinitionMethods
¶ Bases:
object
Used to indicate the method being used to define the seam locations.
Not valid for
NXOpen.Features.ShipDesign.SeamBuilderTypes.Intersection
.Enum Members
The intersection or projection of the selected data with the ship structure defines the seam location. “
“EquallySpaced”, ” Create a specified number of seams equidistant between two selected curves. ” “Rectangular”, ” Create a rectangular pattern of seams based on an origin, direction, and size of rectangles. “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-