ReadDataSetBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ReadDataSetBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class will read a data set file from Team Center
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CreateDataSetToggle | Returns or sets the property that if the toggle is on then the native file will be added to current work part as a data set |
DataSets | Returns or sets the index value of the available data set names |
NativeFileBrowser | Returns or sets the file name of the data set from the native file system |
NativeToggle | Returns or sets the flag that represents if toggle is on the a file of the data set type can be retrieved from the Native file system |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetDataSetNames | The list of available data set names under the current work part |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CreateDataSetToggle¶
-
ReadDataSetBuilder.
CreateDataSetToggle
¶ Returns or sets the property that if the toggle is on then the native file will be added to current work part as a data set
-------------------------------------
Getter Method
Signature
CreateDataSetToggle()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateDataSetToggle(createDataSetToggle)
Parameters: createDataSetToggle (bool) – New in version NX8.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
DataSets¶
-
ReadDataSetBuilder.
DataSets
¶ Returns or sets the index value of the available data set names
-------------------------------------
Getter Method
Signature
DataSets()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DataSets(dataSets)
Parameters: dataSets (int) – New in version NX8.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
NativeFileBrowser¶
-
ReadDataSetBuilder.
NativeFileBrowser
¶ Returns or sets the file name of the data set from the native file system
-------------------------------------
Getter Method
Signature
NativeFileBrowser()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NativeFileBrowser(filename)
Parameters: filename (str) – New in version NX8.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
NativeToggle¶
-
ReadDataSetBuilder.
NativeToggle
¶ Returns or sets the flag that represents if toggle is on the a file of the data set type can be retrieved from the Native file system
-------------------------------------
Getter Method
Signature
NativeToggle()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NativeToggle(nativeToggle)
Parameters: nativeToggle (bool) – New in version NX8.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
Method Detail¶
GetDataSetNames¶
-
ReadDataSetBuilder.
GetDataSetNames
¶ The list of available data set names under the current work part
Signature
GetDataSetNames()
Returns: Available data set names derived from the input Team Center relations. :rtype: list of str
New in version NX8.5.0.
License requirements: None.
Validate¶
-
ReadDataSetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.