PlateStockBuilderThicknessSourceOptions Enumeration¶
NXOpen.Features.ShipDesign.PlateStockBuilder.ThicknessSourceOptions is an alias for NXOpen.Features.ShipDesign.PlateStockBuilderThicknessSourceOptions
-
class
NXOpen.Features.ShipDesign.
PlateStockBuilderThicknessSourceOptions
¶ Bases:
object
Settings to indicate where the material thickness source resides.
Enum Members
Enum Member Enum Member Description File The thickness is defined by a table of standard thicknesses for different material and material grades in CSV file.List The thickness is defined by a list of standard thicknesses for different material and material grades.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-