PlateChamferBuilderTypes Enumeration¶
NXOpen.Features.ShipDesign.PlateChamferBuilder.Types is an alias for NXOpen.Features.ShipDesign.PlateChamferBuilderTypes
-
class
NXOpen.Features.ShipDesign.
PlateChamferBuilderTypes
¶ Bases:
object
The option for the type of associativity for chamfer.
Enum Members
Enum Member Enum Member Description OnEdge Create a chamfer on the edgeToPlate Create a chamfer on the common edges between plates-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-