PlateChamferBuilderAngleMethod Enumeration¶
NXOpen.Features.ShipDesign.PlateChamferBuilder.AngleMethod is an alias for NXOpen.Features.ShipDesign.PlateChamferBuilderAngleMethod
-
class
NXOpen.Features.ShipDesign.
PlateChamferBuilderAngleMethod
¶ Bases:
object
The option to specify the method for defining angle or ratio.
Enum Members
Enum Member Enum Member Description Angle Use the angle for the chamfer parametersRatio Use the ratio for the chamfer parameters-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-