PillarBuilderStockSectionType Enumeration¶
NXOpen.Features.ShipDesign.PillarBuilder.StockSectionType is an alias for NXOpen.Features.ShipDesign.PillarBuilderStockSectionType
-
class
NXOpen.Features.ShipDesign.
PillarBuilderStockSectionType
¶ Bases:
object
SpreadSheet Type Profile or BuiltUp
Enum Members
Enum Member Enum Member Description Profile Profile StockBuiltUp Built Up Stock-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-