PillarBuilderEndTypeOptions Enumeration¶
NXOpen.Features.ShipDesign.PillarBuilder.EndTypeOptions is an alias for NXOpen.Features.ShipDesign.PillarBuilderEndTypeOptions
-
class
NXOpen.Features.ShipDesign.
PillarBuilderEndTypeOptions
¶ Bases:
object
this specifies end type option
Enum Members
Enum Member Enum Member Description NotSet No end cuts are appliedEndcut The same end cut is applied to both endsCap Each end has different end cuts-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-