PillarBuilderEndCutTypes Enumeration¶
NXOpen.Features.ShipDesign.PillarBuilder.EndCutTypes is an alias for NXOpen.Features.ShipDesign.PillarBuilderEndCutTypes
-
class
NXOpen.Features.ShipDesign.
PillarBuilderEndCutTypes
¶ Bases:
object
this specifies how the end cuts are applied
Enum Members
Enum Member Enum Member Description NotSet No end cuts are appliedSymmetric The same end cut is applied to both endsTwoSided Each end has different end cuts-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-