PenetrationManager Class¶
-
class
NXOpen.Features.ShipDesign.
PenetrationManager
¶ Bases:
object
Contains the collection objects for creating and iterating over Penetration Request Properties objects.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX7.5.1.
“PenetrationUtils”, ” Returns the PenetrationUtils instance ” “PenetrationRequestCollection”, ” Returns the PenetrationRequestCollection instance “
PenetrationUtils¶
-
PenetrationManager.
PenetrationUtils
¶ Returns the PenetrationUtils instance
Signature
PenetrationUtils()
New in version NX8.0.0.
Returns: Return type: NXOpen.Features.ShipDesign.PenetrationUtils
PenetrationRequestCollection¶
-
PenetrationManager.
PenetrationRequestCollection
¶ Returns the PenetrationRequestCollection instance
Signature
PenetrationRequestCollection()
New in version NX8.0.0.
Returns: Return type: NXOpen.Features.ShipDesign.PenetrationRequestCollection