OrientationPointMethodsBuilderPointMethodTypes Enumeration¶
NXOpen.Features.ShipDesign.OrientationPointMethodsBuilder.PointMethodTypes is an alias for NXOpen.Features.ShipDesign.OrientationPointMethodsBuilderPointMethodTypes
-
class
NXOpen.Features.ShipDesign.
OrientationPointMethodsBuilderPointMethodTypes
¶ Bases:
object
Settings to indicate how the boundary is defined.
Enum Members
Enum Member Enum Member Description ByPoint The boundary is defined by a location on the landing curve closest to a specified point.ByDistance The boundary is defined by a distance from a reference object.FromStart The boundary is defined by a distance from the start of the landing curve.FromEnd The boundary is defined by a distance from the end of the landing curve.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-