MirrorShipStructureBuilderTypes Enumeration¶
NXOpen.Features.ShipDesign.MirrorShipStructureBuilder.Types is an alias for NXOpen.Features.ShipDesign.MirrorShipStructureBuilderTypes
-
class
NXOpen.Features.ShipDesign.
MirrorShipStructureBuilderTypes
¶ Bases:
object
Settings to indicate the selection type of ship feature.
Enum Members
Enum Member Enum Member Description StructureSystem The structure system type.Feature The feature type which is valid only in ship basic design application.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-