MirrorShipStructureBuilderAppTypes Enumeration¶
NXOpen.Features.ShipDesign.MirrorShipStructureBuilder.AppTypes is an alias for NXOpen.Features.ShipDesign.MirrorShipStructureBuilderAppTypes
-
class
NXOpen.Features.ShipDesign.
MirrorShipStructureBuilderAppTypes
¶ Bases:
object
Settings to indicate the current application type.
Enum Members
Enum Member Enum Member Description ShipDetailDesign The ship detail design.ShipBasicDesign The ship basic design.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-