InteractiveAnnotationBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
InteractiveAnnotationBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.ShipDesign.InteractiveAnnotationBuilder
builder .This builder returns None. To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateInteractiveAnnotationBuilder()
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
AddAnnotationOfBracket | Add annotation of bracket |
AddAnnotationOfEndCuts | Add annotation of end cuts. |
AddAnnotationOfExpansionPlate | Add annotation of expansion plate |
AddAnnotationOfExpansionStiffenerEndCuts | Add annotation of expansion stiffener endcuts |
AddAnnotationOfExpansionStiffenerSturctureIdAndScantling | Add annotation of structure ID and scantling on Ship Expansion View |
AddAnnotationOfOpeningFillingLine | Add annotation of opening filling line |
AddAnnotationOfSeamForDetailDesign | Add annotation of seam symbol for detail design |
AddAnnotationOfStructureIdAndScantling | Add annotations of sturcture ID And scantling. |
AddFillingLineByChain | Adds opening filling lines by curve chain method. |
AddFillingLineByPoints | Adds opening filling lines by points method. |
Commit | Commits any edits that have been applied to the builder. |
DeleteExistingAnnotations | Deletes the existing annotations excluding the opening filling lines. |
DeleteOpeningFillingLine | Deletes the specific opening filling line. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
HandleAnnotationForBasicDesign | Creates ship annotations for basic design structures. |
HandleSeamForNonSectionedPlateForBasicDesign | Add annotation of seam symbol for non-sectioned plate for basic design |
HandleSeamForSectionedPlateForBasicDesign | Add annotation of seam symbol for sectioned plate for basic design |
ModifyFillingLineByPoints | Modifies the position of opening filling line, which is created by points method. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AddAnnotationOfBracket¶
-
InteractiveAnnotationBuilder.
AddAnnotationOfBracket
¶ Add annotation of bracket
Signature
AddAnnotationOfBracket(createBracketSymbol, draftingbody)
Parameters: - createBracketSymbol (bool) –
- draftingbody (
NXOpen.Drawings.DraftingBody
) –
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
AddAnnotationOfEndCuts¶
-
InteractiveAnnotationBuilder.
AddAnnotationOfEndCuts
¶ Add annotation of end cuts.
Signature
AddAnnotationOfEndCuts(createEndCutsSymbol, draftingBody)
Parameters: - createEndCutsSymbol (bool) – Create End Cuts symbols or not
- draftingBody (
NXOpen.Drawings.DraftingBody
) –
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
AddAnnotationOfExpansionPlate¶
-
InteractiveAnnotationBuilder.
AddAnnotationOfExpansionPlate
¶ Add annotation of expansion plate
Signature
AddAnnotationOfExpansionPlate(tgView, shipStructure, createScantlingAnnotation)
Parameters: - tgView (
NXOpen.Drawings.DraftingView
) – The Ship Expansion View - shipStructure (
NXOpen.NXObject
) – The Ship Structure on that the annotation will create. - createScantlingAnnotation (bool) – Create Scantling Annotation or not
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
- tgView (
AddAnnotationOfExpansionStiffenerEndCuts¶
-
InteractiveAnnotationBuilder.
AddAnnotationOfExpansionStiffenerEndCuts
¶ Add annotation of expansion stiffener endcuts
Signature
AddAnnotationOfExpansionStiffenerEndCuts(tgView, shipStructure, createEndCutsSymbol)
Parameters: - tgView (
NXOpen.Drawings.DraftingView
) – The Ship Expansion View - shipStructure (
NXOpen.NXObject
) – The Ship Structure on that the annotation will create. - createEndCutsSymbol (bool) – Create End Cuts Symbol or not
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
- tgView (
AddAnnotationOfExpansionStiffenerSturctureIdAndScantling¶
-
InteractiveAnnotationBuilder.
AddAnnotationOfExpansionStiffenerSturctureIdAndScantling
¶ Add annotation of structure ID and scantling on Ship Expansion View
Signature
AddAnnotationOfExpansionStiffenerSturctureIdAndScantling(tgView, shipStructure, createIDAnnotation, createScantlingAnnotation)
Parameters: - tgView (
NXOpen.Drawings.DraftingView
) – The Ship Expansion View - shipStructure (
NXOpen.NXObject
) – The Ship Structure on that the annotation will create. - createIDAnnotation (bool) – Create ID annotation or not
- createScantlingAnnotation (bool) – Create Scantling Annotation or not
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
- tgView (
AddAnnotationOfOpeningFillingLine¶
-
InteractiveAnnotationBuilder.
AddAnnotationOfOpeningFillingLine
¶ Add annotation of opening filling line
Signature
AddAnnotationOfOpeningFillingLine(createOpeningFillingLine, draftingbody)
Parameters: - createOpeningFillingLine (bool) –
- draftingbody (
NXOpen.Drawings.DraftingBody
) –
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
AddAnnotationOfSeamForDetailDesign¶
-
InteractiveAnnotationBuilder.
AddAnnotationOfSeamForDetailDesign
¶ Add annotation of seam symbol for detail design
Signature
AddAnnotationOfSeamForDetailDesign(createSeamSymbol, tgView, objects, selectedObjecty)
Parameters: - createSeamSymbol (bool) –
- tgView (
NXOpen.Drawings.DraftingView
) – - objects (list of
NXOpen.Drawings.DraftingBody
) – - selectedObjecty (
NXOpen.Drawings.DraftingBody
) –
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
AddAnnotationOfStructureIdAndScantling¶
-
InteractiveAnnotationBuilder.
AddAnnotationOfStructureIdAndScantling
¶ Add annotations of sturcture ID And scantling.
Signature
AddAnnotationOfStructureIdAndScantling(createIDAnnotation, createScantlingAnnotation, draftingBody)
Parameters: - createIDAnnotation (bool) – Create ID annotation or not
- createScantlingAnnotation (bool) – Create Scantling annotation or not
- draftingBody (
NXOpen.Drawings.DraftingBody
) –
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
AddFillingLineByChain¶
-
InteractiveAnnotationBuilder.
AddFillingLineByChain
¶ Adds opening filling lines by curve chain method.
Signature
AddFillingLineByChain(curves, createChainAnnotation)
Parameters: - curves (list of
NXOpen.Drawings.DraftingCurve
) – Ship drafting curves - createChainAnnotation (bool) – Create Chain Annotation or not
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
- curves (list of
AddFillingLineByPoints¶
-
InteractiveAnnotationBuilder.
AddFillingLineByPoints
¶ Adds opening filling lines by points method.
Signature
AddFillingLineByPoints(spiderPoint, strikingPoint)
Parameters: - spiderPoint (
NXOpen.Point
) – spider point - strikingPoint (
NXOpen.Point
) – striking point
Returns: Create line by points
Return type: New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
- spiderPoint (
DeleteExistingAnnotations¶
-
InteractiveAnnotationBuilder.
DeleteExistingAnnotations
¶ Deletes the existing annotations excluding the opening filling lines.
Signature
DeleteExistingAnnotations()
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
DeleteOpeningFillingLine¶
-
InteractiveAnnotationBuilder.
DeleteOpeningFillingLine
¶ Deletes the specific opening filling line.
Signature
DeleteOpeningFillingLine(line)
Parameters: line ( NXOpen.Line
) –New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
HandleAnnotationForBasicDesign¶
-
InteractiveAnnotationBuilder.
HandleAnnotationForBasicDesign
¶ Creates ship annotations for basic design structures.
Signature
HandleAnnotationForBasicDesign(createIDAnnotation, createScantlingAnnotation, createEndCutsAnnotation, draftingVDCurve, shipEntity, view)
Parameters: - createIDAnnotation (bool) – Create Structure ID Annotation or not
- createScantlingAnnotation (bool) – Create Scantling Annotation or not
- createEndCutsAnnotation (bool) – Create EndCuts Annotation or not
- draftingVDCurve (
NXOpen.Drawings.DraftingCurve
) – Ship drafting curve - shipEntity (
NXOpen.NXObject
) – The ship entity, entity type can beNXOpen.Body
orNXOpen.Face
- view (
NXOpen.Drawings.DraftingView
) – Ship drafting section view
Returns: The ship entity annotation, entity type can be
NXOpen.Body
orNXOpen.Face
Return type: New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
HandleSeamForNonSectionedPlateForBasicDesign¶
-
InteractiveAnnotationBuilder.
HandleSeamForNonSectionedPlateForBasicDesign
¶ Add annotation of seam symbol for non-sectioned plate for basic design
Signature
HandleSeamForNonSectionedPlateForBasicDesign(createSeamSymbol, draftingVDCurve, tgCurve)
Parameters: - createSeamSymbol (bool) –
- draftingVDCurve (
NXOpen.Drawings.DraftingCurve
) – Ship drafting curve - tgCurve (
NXOpen.NXObject
) –
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
HandleSeamForSectionedPlateForBasicDesign¶
-
InteractiveAnnotationBuilder.
HandleSeamForSectionedPlateForBasicDesign
¶ Add annotation of seam symbol for sectioned plate for basic design
Signature
HandleSeamForSectionedPlateForBasicDesign(createSeamSymbol, tgDraftingBody, objects, selectedObject)
Parameters: - createSeamSymbol (bool) –
- tgDraftingBody (
NXOpen.Drawings.DraftingBody
) – - objects (list of
NXOpen.Drawings.DraftingCurve
) – - selectedObject (
NXOpen.Drawings.DraftingCurve
) –
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
ModifyFillingLineByPoints¶
-
InteractiveAnnotationBuilder.
ModifyFillingLineByPoints
¶ Modifies the position of opening filling line, which is created by points method.
Signature
ModifyFillingLineByPoints(spiderPoint, strikingPoint, line)
Parameters: - spiderPoint (
NXOpen.Point
) – spider point - strikingPoint (
NXOpen.Point
) – striking point - line (
NXOpen.Line
) – line which created by point
New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
- spiderPoint (
Validate¶
-
InteractiveAnnotationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.