ExcessMaterialBuilderVersionID Enumeration¶
NXOpen.Features.ShipDesign.ExcessMaterialBuilder.VersionID is an alias for NXOpen.Features.ShipDesign.ExcessMaterialBuilderVersionID
-
class
NXOpen.Features.ShipDesign.
ExcessMaterialBuilderVersionID
¶ Bases:
object
version identifiers for the different revisions of the excess material feature.
Enum Members
Enum Member Enum Member Description Original This feature builder is used to edit an existing NX75 - NX901 excess material feature.Nx902 This feature builder is used to create or edit an NX902 or beyond feature.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-