EndCutBuilderSelectionTypes Enumeration¶
NXOpen.Features.ShipDesign.EndCutBuilder.SelectionTypes is an alias for NXOpen.Features.ShipDesign.EndCutBuilderSelectionTypes
-
class
NXOpen.Features.ShipDesign.
EndCutBuilderSelectionTypes
¶ Bases:
object
This enum defines the Placement Face and Placement Edge Selection Type.
Enum Members
All faces specified as placement faces must have valid attributes that identify it as a valid face for Endcuts.
- “
- “FaceAndEdge”, ” If this Selection Type is set, then a single pair of a Face (Placement Face) and an edge(Placement Edge) needs to be specified. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.