EndCutBuilderDraftTypes Enumeration¶
NXOpen.Features.ShipDesign.EndCutBuilder.DraftTypes is an alias for NXOpen.Features.ShipDesign.EndCutBuilderDraftTypes
-
class
NXOpen.Features.ShipDesign.
EndCutBuilderDraftTypes
¶ Bases:
object
This enum defines the types of draft to be applied.
Enum Members
Enum Member Enum Member Description Trim If this Draft Type is set, the EndCut face will split and the left side face will be tapered.Extend If this Draft Type is set, the EndCut face will split and the right side face will be tapered.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-