DrawingAnnotationBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
DrawingAnnotationBuilder
¶ Bases:
NXOpen.Builder
This builder allows you to define the drawing annotation information.
It represents
NXOpen.Features.ShipDesign.DrawingAnnotationBuilder
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateDrawingAnnotationBuilder()
Default values.
Property Value ExistingAutomaticAnnotation Preserve IsCreateOpeningFillLines 1 IsCreateScantling 1 IsCreateScantlingTable 1 IsCreateStructureID 0 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ExistingAutomaticAnnotation | Returns or sets the option specify how to handle existing annotation |
IsCreateContinuitySymbolOnSectionStiffener | Returns or sets the setting that indicates whether continuity symbol on section stiffener will be created for the ship objects |
IsCreateOpeningFillLines | Returns or sets the setting that indicates whether opening fill lines will be created for ship objects |
IsCreateScantling | Returns or sets the setting that indicates whether scantling will be created for the ship objects |
IsCreateScantlingTable | Returns or sets the setting that indicates whether the most common scantlings for stiffener and plate will be created for the view. |
IsCreateStiffenerSectionSymbol | Returns or sets the setting that indicates whether the section symbol will be created for stiffeners |
IsCreateStructureID | Returns or sets the setting that indicates whether structure id will be created for ship objects |
Tag | Returns the Tag for this object. |
ViewList | Returns the drafting views to be annotated |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DrawingAnnotationBuilderAnnotation Enumeration | Settings that indicate how to handle the exsiting annotation in the drawing. |
Property Detail¶
ExistingAutomaticAnnotation¶
-
DrawingAnnotationBuilder.
ExistingAutomaticAnnotation
¶ Returns or sets the option specify how to handle existing annotation
-------------------------------------
Getter Method
Signature
ExistingAutomaticAnnotation()
Returns: Return type: NXOpen.Features.ShipDesign.DrawingAnnotationBuilderAnnotation
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExistingAutomaticAnnotation(existingAutomaticAnnotation)
Parameters: existingAutomaticAnnotation ( NXOpen.Features.ShipDesign.DrawingAnnotationBuilderAnnotation
) –New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
IsCreateContinuitySymbolOnSectionStiffener¶
-
DrawingAnnotationBuilder.
IsCreateContinuitySymbolOnSectionStiffener
¶ Returns or sets the setting that indicates whether continuity symbol on section stiffener will be created for the ship objects
-------------------------------------
Getter Method
Signature
IsCreateContinuitySymbolOnSectionStiffener()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCreateContinuitySymbolOnSectionStiffener(isCreateContinuitySymbolOnSectionStiffener)
Parameters: isCreateContinuitySymbolOnSectionStiffener (bool) – New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
IsCreateOpeningFillLines¶
-
DrawingAnnotationBuilder.
IsCreateOpeningFillLines
¶ Returns or sets the setting that indicates whether opening fill lines will be created for ship objects
-------------------------------------
Getter Method
Signature
IsCreateOpeningFillLines()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCreateOpeningFillLines(isCreateOpeningFillLines)
Parameters: isCreateOpeningFillLines (bool) – New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
IsCreateScantling¶
-
DrawingAnnotationBuilder.
IsCreateScantling
¶ Returns or sets the setting that indicates whether scantling will be created for the ship objects
-------------------------------------
Getter Method
Signature
IsCreateScantling()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCreateScantling(isCreateScantling)
Parameters: isCreateScantling (bool) – New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
IsCreateScantlingTable¶
-
DrawingAnnotationBuilder.
IsCreateScantlingTable
¶ Returns or sets the setting that indicates whether the most common scantlings for stiffener and plate will be created for the view.
If yes, the stiffener and plate scantlings, other than the most common one, will not be created.
-------------------------------------
Getter Method
Signature
IsCreateScantlingTable()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCreateScantlingTable(isCreateScantlingTable)
Parameters: isCreateScantlingTable (bool) – New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
IsCreateStiffenerSectionSymbol¶
-
DrawingAnnotationBuilder.
IsCreateStiffenerSectionSymbol
¶ Returns or sets the setting that indicates whether the section symbol will be created for stiffeners
-------------------------------------
Getter Method
Signature
IsCreateStiffenerSectionSymbol()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCreateStiffenerSectionSymbol(isCreateStiffenerSectionSymbol)
Parameters: isCreateStiffenerSectionSymbol (bool) – New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
IsCreateStructureID¶
-
DrawingAnnotationBuilder.
IsCreateStructureID
¶ Returns or sets the setting that indicates whether structure id will be created for ship objects
-------------------------------------
Getter Method
Signature
IsCreateStructureID()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCreateStructureID(isCreateStructureID)
Parameters: isCreateStructureID (bool) – New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
ViewList¶
-
DrawingAnnotationBuilder.
ViewList
¶ Returns the drafting views to be annotated
-------------------------------------
Getter Method
Signature
ViewList()
Returns: Return type: NXOpen.Drawings.SelectDraftingViewList
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
DrawingAnnotationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.