DeckBuilderTypes Enumeration¶
NXOpen.Features.ShipDesign.DeckBuilder.Types is an alias for NXOpen.Features.ShipDesign.DeckBuilderTypes
-
class
NXOpen.Features.ShipDesign.
DeckBuilderTypes
¶ Bases:
object
Indicates the method that is being used to define the mold face of the deck.
Enum Members
Enum Member Enum Member Description SheetBody Mold face is being defined by a selected sheet body.Planes Mold face is being defined by selected or defined planes.RoundCamber Mold face is being defined by a generated round camber shape.StraightCamber Mold face is being defined by a generated straight camber shape.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-