CuttingSideFacesBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
CuttingSideFacesBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Used to create a
NXOpen.Features.ShipDesign.CuttingSideFacesBuilder
which is used to attribute the cutting side, and opposing cutting side, faces on the plate bodies.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateCuttingSideFacesBuilder()
Default values.
Property Value ProcessCoplanar 1 ProcessTangent 1 ReverseSide 0 TangentFaceThreshold.Value 15 WeldGapThreshold.Value 0 (millimeters part), 0 (inches part) New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
CuttingSideFaces | Returns the faces to identify, or attribute, as cutting side. |
DistanceTolerance | Returns or sets the modeling distance tolerance. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProcessCoplanar | Returns or sets the option identifying if a coplanar rule should be applied to find cutting side faces. |
ProcessTangent | Returns or sets the option identifying if a tangent rule should be applied to find adjacent cutting side faces. |
ReverseSide | Returns or sets the value to decide if the normal face assignment should be done to the opposite side. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TangentFaceThreshold | Returns the value (in degrees) to determine if adjacent surfaces are tangent. |
Type | Returns or sets the value for how to process the bodies and faces. |
WeldGapThreshold | Returns the maximum distance the profile, or another plate, can be from the selected plate face. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CuttingSideFacesBuilderTypes Enumeration | Type of operation to perform on the plate. |
Property Detail¶
CuttingSideFaces¶
-
CuttingSideFacesBuilder.
CuttingSideFaces
¶ Returns the faces to identify, or attribute, as cutting side.
-------------------------------------
Getter Method
Signature
CuttingSideFaces()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
DistanceTolerance¶
-
CuttingSideFacesBuilder.
DistanceTolerance
¶ Returns or sets the modeling distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
ProcessCoplanar¶
-
CuttingSideFacesBuilder.
ProcessCoplanar
¶ Returns or sets the option identifying if a coplanar rule should be applied to find cutting side faces.
No limitiations are placed on adjacency of the faces (they can be far away from each other).
-------------------------------------
Getter Method
Signature
ProcessCoplanar()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProcessCoplanar(processCoplanar)
Parameters: processCoplanar (bool) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
ProcessTangent¶
-
CuttingSideFacesBuilder.
ProcessTangent
¶ Returns or sets the option identifying if a tangent rule should be applied to find adjacent cutting side faces.
Faces must be adjacent and within the modeling distance tolerance.
-------------------------------------
Getter Method
Signature
ProcessTangent()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProcessTangent(processTangent)
Parameters: processTangent (bool) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
ReverseSide¶
-
CuttingSideFacesBuilder.
ReverseSide
¶ Returns or sets the value to decide if the normal face assignment should be done to the opposite side.
-------------------------------------
Getter Method
Signature
ReverseSide()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseSide(reverseSide)
Parameters: reverseSide (bool) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
TangentFaceThreshold¶
-
CuttingSideFacesBuilder.
TangentFaceThreshold
¶ Returns the value (in degrees) to determine if adjacent surfaces are tangent.
-------------------------------------
Getter Method
Signature
TangentFaceThreshold()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Type¶
-
CuttingSideFacesBuilder.
Type
¶ Returns or sets the value for how to process the bodies and faces.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Features.ShipDesign.CuttingSideFacesBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Features.ShipDesign.CuttingSideFacesBuilderTypes
) –New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
WeldGapThreshold¶
-
CuttingSideFacesBuilder.
WeldGapThreshold
¶ Returns the maximum distance the profile, or another plate, can be from the selected plate face.
-------------------------------------
Getter Method
Signature
WeldGapThreshold()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CuttingSideFacesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.