CustomBracketBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
CustomBracketBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.CustomBracket
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateCustomBracketBuilder()
Default values.
Property Value SketchBlock.Exp1.Value 0 SketchBlock.Exp10.Value 0 SketchBlock.Exp11.Value 0 SketchBlock.Exp12.Value 0 SketchBlock.Exp2.Value 0 SketchBlock.Exp3.Value 0 SketchBlock.Exp4.Value 0 SketchBlock.Exp5.Value 0 SketchBlock.Exp6.Value 0 SketchBlock.Exp7.Value 0 SketchBlock.Exp8.Value 0 SketchBlock.Exp9.Value 0 SketchBlock.Sketches EndCut1 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AttributeMaterial | Returns or sets the material attribute |
AttributeName | Returns or sets the name attribute value |
CoordSystem | Returns or sets the placement csys of the bracket |
HeelOffset | Returns the heel offset |
HeelPoint | Returns or sets the heel point |
KeepCoordSystem | Returns or sets the toggle which allows re-use of the previous coordinate system |
KeepHeelPoint | Returns or sets the toggle which allows re-use of the previous heel point |
KeepPlacementPlane | Returns or sets the toggle which allows re-use of the previous placement plane |
KeepReferencePlane | Returns or sets the toggle which allows re-use of the previous reference plane |
KeepReverseDirection | Returns or sets the toggle which allows re-use of the previous flip direction toggle |
KeepSelectTrimFace | Returns or sets the keep select trim face A toggle used to remember the selected object(s) on apply. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlacementPlane | Returns or sets the placement plane |
PlacementType | Returns or sets the method used to define the placement of the bracket |
ReferencePlane | Returns or sets the reference plane |
ReverseDirection | Returns or sets the flip direction toggle for the extrude direction |
SelectTrimFace | Returns the select trim face. |
SketchBlock | Returns the sketch block |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Thickness | Returns the thickness of the bracket |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAvailableAttributeMaterials | Returns the list of available material attributes @return Array of available attribute materials. |
GetAvailableAttributeNames | Returns the list of available name attributes @return Array of available attribute names. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CustomBracketBuilderCreationMethod Enumeration | Creation method used to define the placement of the bracket |
Property Detail¶
AttributeMaterial¶
-
CustomBracketBuilder.
AttributeMaterial
¶ Returns or sets the material attribute
-------------------------------------
Getter Method
Signature
AttributeMaterial()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttributeMaterial(material)
Parameters: material (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
AttributeName¶
-
CustomBracketBuilder.
AttributeName
¶ Returns or sets the name attribute value
-------------------------------------
Getter Method
Signature
AttributeName()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttributeName(name)
Parameters: name (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
CoordSystem¶
-
CustomBracketBuilder.
CoordSystem
¶ Returns or sets the placement csys of the bracket
-------------------------------------
Getter Method
Signature
CoordSystem()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordSystem(coordSystem)
Parameters: coordSystem ( NXOpen.CoordinateSystem
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
HeelOffset¶
-
CustomBracketBuilder.
HeelOffset
¶ Returns the heel offset
-------------------------------------
Getter Method
Signature
HeelOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
HeelPoint¶
-
CustomBracketBuilder.
HeelPoint
¶ Returns or sets the heel point
-------------------------------------
Getter Method
Signature
HeelPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeelPoint(heelPoint)
Parameters: heelPoint ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepCoordSystem¶
-
CustomBracketBuilder.
KeepCoordSystem
¶ Returns or sets the toggle which allows re-use of the previous coordinate system
-------------------------------------
Getter Method
Signature
KeepCoordSystem()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepCoordSystem(keepCoordSystem)
Parameters: keepCoordSystem (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepHeelPoint¶
-
CustomBracketBuilder.
KeepHeelPoint
¶ Returns or sets the toggle which allows re-use of the previous heel point
-------------------------------------
Getter Method
Signature
KeepHeelPoint()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepHeelPoint(keepHeelPoint)
Parameters: keepHeelPoint (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepPlacementPlane¶
-
CustomBracketBuilder.
KeepPlacementPlane
¶ Returns or sets the toggle which allows re-use of the previous placement plane
-------------------------------------
Getter Method
Signature
KeepPlacementPlane()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepPlacementPlane(keepPlacementPlane)
Parameters: keepPlacementPlane (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepReferencePlane¶
-
CustomBracketBuilder.
KeepReferencePlane
¶ Returns or sets the toggle which allows re-use of the previous reference plane
-------------------------------------
Getter Method
Signature
KeepReferencePlane()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepReferencePlane(keepReferencePlane)
Parameters: keepReferencePlane (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepReverseDirection¶
-
CustomBracketBuilder.
KeepReverseDirection
¶ Returns or sets the toggle which allows re-use of the previous flip direction toggle
-------------------------------------
Getter Method
Signature
KeepReverseDirection()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepReverseDirection(keepReverseDirection)
Parameters: keepReverseDirection (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepSelectTrimFace¶
-
CustomBracketBuilder.
KeepSelectTrimFace
¶ Returns or sets the keep select trim face A toggle used to remember the selected object(s) on apply.
-------------------------------------
Getter Method
Signature
KeepSelectTrimFace()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepSelectTrimFace(keepSelectTrimFace)
Parameters: keepSelectTrimFace (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
PlacementPlane¶
-
CustomBracketBuilder.
PlacementPlane
¶ Returns or sets the placement plane
-------------------------------------
Getter Method
Signature
PlacementPlane()
Returns: Return type: NXOpen.Plane
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlacementPlane(placementPlane)
Parameters: placementPlane ( NXOpen.Plane
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
PlacementType¶
-
CustomBracketBuilder.
PlacementType
¶ Returns or sets the method used to define the placement of the bracket
-------------------------------------
Getter Method
Signature
PlacementType()
Returns: Return type: NXOpen.Features.ShipDesign.CustomBracketBuilderCreationMethod
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlacementType(placementType)
Parameters: placementType ( NXOpen.Features.ShipDesign.CustomBracketBuilderCreationMethod
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
ReferencePlane¶
-
CustomBracketBuilder.
ReferencePlane
¶ Returns or sets the reference plane
-------------------------------------
Getter Method
Signature
ReferencePlane()
Returns: Return type: NXOpen.Plane
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePlane(referencePlane)
Parameters: referencePlane ( NXOpen.Plane
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
ReverseDirection¶
-
CustomBracketBuilder.
ReverseDirection
¶ Returns or sets the flip direction toggle for the extrude direction
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
SelectTrimFace¶
-
CustomBracketBuilder.
SelectTrimFace
¶ Returns the select trim face.
Specifies the face(s) to cut holes in.
-------------------------------------
Getter Method
Signature
SelectTrimFace()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
SketchBlock¶
-
CustomBracketBuilder.
SketchBlock
¶ Returns the sketch block
-------------------------------------
Getter Method
Signature
SketchBlock()
Returns: Return type: NXOpen.SketchExpressionModifierBuilder
New in version NX7.5.0.
License requirements: None.
Thickness¶
-
CustomBracketBuilder.
Thickness
¶ Returns the thickness of the bracket
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Method Detail¶
GetAvailableAttributeMaterials¶
-
CustomBracketBuilder.
GetAvailableAttributeMaterials
¶ Returns the list of available material attributes
Signature
GetAvailableAttributeMaterials()
Returns: Array of available attribute materials. These materials are specified in the customer defaults file. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableAttributeNames¶
-
CustomBracketBuilder.
GetAvailableAttributeNames
¶ Returns the list of available name attributes
Signature
GetAvailableAttributeNames()
Returns: Array of available attribute names. These names are specified in the customer defaults file. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
Validate¶
-
CustomBracketBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.