CornerCutListItemBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
CornerCutListItemBuilder
¶ Bases:
NXOpen.Builder
Used to supply the list of corner cut locations and seam curves to the
NXOpen.Features.ShipDesign.CornerCutBuilder
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateCornerCutListitemBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CornerPoint | Returns or sets the corner point as the cut location. |
SeamCurve | Returns the seam curve to resize the corner cut. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CornerPoint¶
-
CornerCutListItemBuilder.
CornerPoint
¶ Returns or sets the corner point as the cut location.
The corner point is used only when the placement type is using corner.
-------------------------------------
Getter Method
Signature
CornerPoint()
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerPoint(weldLocation)
Parameters: weldLocation ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
SeamCurve¶
-
CornerCutListItemBuilder.
SeamCurve
¶ Returns the seam curve to resize the corner cut.
-------------------------------------
Getter Method
Signature
SeamCurve()
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
CornerCutListItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.