ThreeBendCornerBuilderTreatmentTypeOptions Enumeration

NXOpen.Features.SheetMetal.ThreeBendCornerBuilder.TreatmentTypeOptions is an alias for NXOpen.Features.SheetMetal.ThreeBendCornerBuilderTreatmentTypeOptions

class NXOpen.Features.SheetMetal.ThreeBendCornerBuilderTreatmentTypeOptions

Bases: object

This enum represents the corner treatment type.

Enum Members

Enum Member Enum Member Description
Open  
Closed  
CircularCutout  
UCutout  
VCutout  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.