TabBuilderThicknessSideOptions Enumeration¶
NXOpen.Features.SheetMetal.TabBuilder.ThicknessSideOptions is an alias for NXOpen.Features.SheetMetal.TabBuilderThicknessSideOptions
-
class
NXOpen.Features.SheetMetal.
TabBuilderThicknessSideOptions
¶ Bases:
object
This enum represents the extent direction for the Tab.
Enum Members
Enum Member Enum Member Description SectionNormalSide Material created on the side of the section normal.SectionReverseNormalSide Material created on the side opposite to that of the section normal-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-