SheetmetalManagerTabType Enumeration¶
-
class
NXOpen.Features.SheetMetal.
SheetmetalManagerTabType
¶ Bases:
object
This is the enum for Tab type i.
- base tab and secondary tab.
Enum Members
Enum Member Enum Member Description Base base tabSecondary secondary tab-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.