MiterOptionsPositionOptions Enumeration¶
NXOpen.Features.SheetMetal.MiterOptions.PositionOptions is an alias for NXOpen.Features.SheetMetal.MiterOptionsPositionOptions
-
class
NXOpen.Features.SheetMetal.
MiterOptionsPositionOptions
¶ Bases:
object
the miter positions options.
Enum Members
Enum Member Enum Member Description NotSet no miterStart miter is done at the beginningEnd miter is done at the endingBoth miter is done both at beginning and ending-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-