MiterOptionsCornerTreatmentOriginTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.MiterOptions.CornerTreatmentOriginTypeOptions is an alias for NXOpen.Features.SheetMetal.MiterOptionsCornerTreatmentOriginTypeOptions
-
class
NXOpen.Features.SheetMetal.
MiterOptionsCornerTreatmentOriginTypeOptions
¶ Bases:
object
This enum represents corner treatment cutout origin type
Enum Members
Enum Member Enum Member Description BendCenter The cutout origin will be at the intersection of first bend’s centerline and bisector of corner angle.CornerPoint The cutout origin will be at the corner point.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-