HemFlangeBuilderTypeOptions Enumeration

NXOpen.Features.SheetMetal.HemFlangeBuilder.TypeOptions is an alias for NXOpen.Features.SheetMetal.HemFlangeBuilderTypeOptions

class NXOpen.Features.SheetMetal.HemFlangeBuilderTypeOptions

Bases: object

Represents the Hem Flange type.

Enum Members

Enum Member Enum Member Description
ClosedHemType
OpenHemType
SFlangeHemType
CurlHemType  
OpenLoopHemType  
ClosedLoopHemType  
CenteredLoopHemType
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.