GussetBuilderTypes Enumeration¶
NXOpen.Features.SheetMetal.GussetBuilder.Types is an alias for NXOpen.Features.SheetMetal.GussetBuilderTypes
-
class
NXOpen.Features.SheetMetal.
GussetBuilderTypes
¶ Bases:
object
This enum represents the two Gusset Feature types.
Enum Members
Enum Member Enum Member Description AutomaticProfile Gusset(s) will be created between the planar faces adjacent to the selected bend face.UserDefinedProfile Gusset will be created using a profile defined by the user.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-