FlatSolidBuilderTransformComponentsOption Enumeration¶
NXOpen.Features.SheetMetal.FlatSolidBuilder.TransformComponentsOption is an alias for NXOpen.Features.SheetMetal.FlatSolidBuilderTransformComponentsOption
-
class
NXOpen.Features.SheetMetal.
FlatSolidBuilderTransformComponentsOption
¶ Bases:
object
The enum defines how to represent PCB components on flat solid.
New in version NX10.0.0.
Enum Members
Enum Member Enum Member Description NotSet do not transform componentsBody transform components as bodiesCsys transform components as CSYS-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-