FlangeBuilderOffsetTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.FlangeBuilder.OffsetTypeOptions is an alias for NXOpen.Features.SheetMetal.FlangeBuilderOffsetTypeOptions
-
class
NXOpen.Features.SheetMetal.
FlangeBuilderOffsetTypeOptions
¶ Bases:
object
This enum represents the offset type for the flange.
Enum Members
Enum Member Enum Member Description Inside The flange is offset to the inside of the faceOutside The flange is offset to the outside of the face-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-