FlangeBuilderLengthTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.FlangeBuilder.LengthTypeOptions is an alias for NXOpen.Features.SheetMetal.FlangeBuilderLengthTypeOptions
-
class
NXOpen.Features.SheetMetal.
FlangeBuilderLengthTypeOptions
¶ Bases:
object
This enum indicates the two ways that the flange length can be measured.
Enum Members
Enum Member Enum Member Description InsideDimension The flange length is dimensioned to the Inner Mold line.OutsideDimension The flange length is dimensioned to the Outer Mold Line.WebDimension The flange length is dimensioned to the Bend Tangent Line.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-