EditCornerBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
EditCornerBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.SheetMetal.EditCornerBuilder
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateEditCornerBuilder()
Default values.
Property Value BendClosureType Open CornerReliefType None Diameter.Value 2.5 (millimeters part), 0.1 (inches part) OverlapRatio.Value 1 PlateClosureType Closed PlateGap.Value 0 (millimeters part), 0 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BendClosureType | Returns or sets the bend type |
CornerReliefType | Returns or sets the corner relief type |
Diameter | Returns the diameter for a circular cutout |
OverlapRatio | Returns the overlap ratio between plates |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlateClosureType | Returns or sets the plate type |
PlateGap | Returns the gap value between plates |
ReverseOverlap | Returns or sets whether the overlap is reversed or not |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddFacePair | Add a face pair. |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFacePair | Return the face pair. |
GetFeature | Returns the feature currently being edited by this builder. |
GetNumberOfFacePairs | Returns the number of face pairs already identified for the three bend corner feature. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
RemoveFacePair | Removes a face pair (that represents a unique corner) from the list of face pairs already added. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EditCornerBuilderBendClosureTypeOptions Enumeration | This enum specifies the type of bend closure required at the corner. |
EditCornerBuilderCornerReliefTypeOptions Enumeration | This enum specifies the type of relief required at the corner. |
EditCornerBuilderPlateClosureTypeOptions Enumeration | This enum specifies the type of plate closure required at the corner. |
Property Detail¶
BendClosureType¶
-
EditCornerBuilder.
BendClosureType
¶ Returns or sets the bend type
-------------------------------------
Getter Method
Signature
BendClosureType()
Returns: Return type: NXOpen.Features.SheetMetal.EditCornerBuilderBendClosureTypeOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BendClosureType(bends)
Parameters: bends ( NXOpen.Features.SheetMetal.EditCornerBuilderBendClosureTypeOptions
) –New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
CornerReliefType¶
-
EditCornerBuilder.
CornerReliefType
¶ Returns or sets the corner relief type
-------------------------------------
Getter Method
Signature
CornerReliefType()
Returns: Return type: NXOpen.Features.SheetMetal.EditCornerBuilderCornerReliefTypeOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerReliefType(cornerRelief)
Parameters: cornerRelief ( NXOpen.Features.SheetMetal.EditCornerBuilderCornerReliefTypeOptions
) –New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Diameter¶
-
EditCornerBuilder.
Diameter
¶ Returns the diameter for a circular cutout
-------------------------------------
Getter Method
Signature
Diameter()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
OverlapRatio¶
-
EditCornerBuilder.
OverlapRatio
¶ Returns the overlap ratio between plates
-------------------------------------
Getter Method
Signature
OverlapRatio()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
PlateClosureType¶
-
EditCornerBuilder.
PlateClosureType
¶ Returns or sets the plate type
-------------------------------------
Getter Method
Signature
PlateClosureType()
Returns: Return type: NXOpen.Features.SheetMetal.EditCornerBuilderPlateClosureTypeOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlateClosureType(plates)
Parameters: plates ( NXOpen.Features.SheetMetal.EditCornerBuilderPlateClosureTypeOptions
) –New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
PlateGap¶
-
EditCornerBuilder.
PlateGap
¶ Returns the gap value between plates
-------------------------------------
Getter Method
Signature
PlateGap()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ReverseOverlap¶
-
EditCornerBuilder.
ReverseOverlap
¶ Returns or sets whether the overlap is reversed or not
-------------------------------------
Getter Method
Signature
ReverseOverlap()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseOverlap(reverseOverlap)
Parameters: reverseOverlap (bool) – New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
Method Detail¶
AddFacePair¶
-
EditCornerBuilder.
AddFacePair
¶ Add a face pair.
Signature
AddFacePair(firstFace, secondFace)
Parameters: - firstFace (
NXOpen.Face
) – A bend face from a bend - secondFace (
NXOpen.Face
) – A bend face from an adjacent bend
New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
- firstFace (
GetFacePair¶
-
EditCornerBuilder.
GetFacePair
¶ Return the face pair.
Signature
GetFacePair(index)
Parameters: index (int) – Index of the desired face pair Returns: a tuple Return type: A tuple consisting of (firstFace, secondFace). firstFace is a NXOpen.Face
. First face of the face pair secondFace is aNXOpen.Face
. Second face of the face pairNew in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
GetNumberOfFacePairs¶
-
EditCornerBuilder.
GetNumberOfFacePairs
¶ Returns the number of face pairs already identified for the three bend corner feature.
Signature
GetNumberOfFacePairs()
Returns: The number of face pairs currently identified Return type: int New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
RemoveFacePair¶
-
EditCornerBuilder.
RemoveFacePair
¶ Removes a face pair (that represents a unique corner) from the list of face pairs already added.
Signature
RemoveFacePair(firstFace, secondFace)
Parameters: - firstFace (
NXOpen.Face
) – A face from an already selected face pair - secondFace (
NXOpen.Face
) – The other face from the face pair
New in version NX7.5.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”)
- firstFace (
Validate¶
-
EditCornerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.