ConvertToSheetmetalBuilderBendReliefTypeOptions Enumeration

NXOpen.Features.SheetMetal.ConvertToSheetmetalBuilder.BendReliefTypeOptions is an alias for NXOpen.Features.SheetMetal.ConvertToSheetmetalBuilderBendReliefTypeOptions

class NXOpen.Features.SheetMetal.ConvertToSheetmetalBuilderBendReliefTypeOptions

Bases: object

This enum represents the bend relief type.

Enum Members

Enum Member Enum Member Description
NotSet  
Square  
Round  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.