BridgeTransitionBuilderTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.BridgeTransitionBuilder.TypeOptions is an alias for NXOpen.Features.SheetMetal.BridgeTransitionBuilderTypeOptions
-
class
NXOpen.Features.SheetMetal.
BridgeTransitionBuilderTypeOptions
¶ Bases:
object
Enum representing types for Bridge Transition feature.
Enum Members
Enum Member Enum Member Description Zu Bridge Transition type consisting of Bend-Planar-Bend regions.Fold Bridge Transition type consisting of Planar-Bend-Planar regions.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-