BridgeTransitionBuilderInsetOptions Enumeration¶
NXOpen.Features.SheetMetal.BridgeTransitionBuilder.InsetOptions is an alias for NXOpen.Features.SheetMetal.BridgeTransitionBuilderInsetOptions
-
class
NXOpen.Features.SheetMetal.
BridgeTransitionBuilderInsetOptions
¶ Bases:
object
Enum representing the side of the Bridge Transition material with respect to the specified tangent plane.
If it is
Features.SheetMetal.BridgeTransitionBuilderInsetOptions.MaterialInside
then the transtion and start edge flow will be on the same logical side of the plane. If they are on opposite sides then useFeatures.SheetMetal.BridgeTransitionBuilderInsetOptions.MaterialOutside
.Enum Members
Enum Member Enum Member Description MaterialInside Bridge Transition body near tangential plane and start will be on same side of the tangential plane selected.MaterialOutside Bridge Transition body near tangential plane and start will be on opposite sides of the tangential plane selected.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-