BridgeTransitionBuilderFoldTransitionTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.BridgeTransitionBuilder.FoldTransitionTypeOptions is an alias for NXOpen.Features.SheetMetal.BridgeTransitionBuilderFoldTransitionTypeOptions
-
class
NXOpen.Features.SheetMetal.
BridgeTransitionBuilderFoldTransitionTypeOptions
¶ Bases:
object
Enum representing the type of
Features.SheetMetal.BridgeTransitionBuilderTypeOptions.Fold
.Features.SheetMetal.BridgeTransitionBuilderTypeOptions.Fold
can be defined by Length or Bend.Enum Members
Enum Member Enum Member Description Length Fold Transition type is Length.Bend Fold Transition type is Bend.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-