BreakCornerBuilderTypeOptions Enumeration

NXOpen.Features.SheetMetal.BreakCornerBuilder.TypeOptions is an alias for NXOpen.Features.SheetMetal.BreakCornerBuilderTypeOptions

class NXOpen.Features.SheetMetal.BreakCornerBuilderTypeOptions

Bases: object

This enum represents the break corner type.

Enum Members

Enum Member Enum Member Description
Fillet  
ChamferEqualSetback  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.