BendTaperBuilderStartType Enumeration¶
NXOpen.Features.SheetMetal.BendTaperBuilder.StartType is an alias for NXOpen.Features.SheetMetal.BendTaperBuilderStartType
-
class
NXOpen.Features.SheetMetal.
BendTaperBuilderStartType
¶ Bases:
object
This enum represents the start types for the bend taper.
New in version NX10.0.0.
Enum Members
Enum Member Enum Member Description TaperFromBend Taper from BendTaperFromWeb Taper from Web-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-