BendBuilderFixedSideOptions Enumeration¶
NXOpen.Features.SheetMetal.BendBuilder.FixedSideOptions is an alias for NXOpen.Features.SheetMetal.BendBuilderFixedSideOptions
-
class
NXOpen.Features.SheetMetal.
BendBuilderFixedSideOptions
¶ Bases:
object
This enum represents the Fixed Side for Bend.
New in version NX5.0.0.
Enum Members
Enum Member Enum Member Description SectionSideLeft Side pointed to by the inverse of the tangent cross normal vectorSectionSideRight Side pointed to by the tangent cross normal vector-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-