ApplicationContext Enumeration¶
-
class
NXOpen.Features.SheetMetal.
ApplicationContext
¶ Bases:
object
This is the enum representing application context of the feature Enum Members
Enum Member Enum Member Description NxSheetMetal Sheet Metal application contextFlexiblePrintedCircuitDesign Flexible Printed Circuit Design application contextAerospaceSheetMetal Aerospace Sheet Metal application context-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-