AeroJoggleBuilderSideType Enumeration¶
NXOpen.Features.SheetMetal.AeroJoggleBuilder.SideType is an alias for NXOpen.Features.SheetMetal.AeroJoggleBuilderSideType
-
class
NXOpen.Features.SheetMetal.
AeroJoggleBuilderSideType
¶ Bases:
object
This enum defines the side of a twin joggle only side1 is used for a single joggle
Enum Members
Enum Member Enum Member Description Side1 Side 1 (only side of single)Side2 Side 2-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-