AeroFlangeBuilderCompType Enumeration¶
NXOpen.Features.SheetMetal.AeroFlangeBuilder.CompType is an alias for NXOpen.Features.SheetMetal.AeroFlangeBuilderCompType
-
class
NXOpen.Features.SheetMetal.
AeroFlangeBuilderCompType
¶ Bases:
object
This method defines the types of Flange Compensation
Enum Members
Enum Member Enum Member Description Automatic AutomaticAngle AngleDistance DistanceNotSet None-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-