SectionSurfaceBuilderExUDegreeType Enumeration

NXOpen.Features.SectionSurfaceBuilderEx.UDegreeType is an alias for NXOpen.Features.SectionSurfaceBuilderExUDegreeType

class NXOpen.Features.SectionSurfaceBuilderExUDegreeType

Bases: object

Surface Degree type.

Enum Members

Enum Member Enum Member Description
Conic
conic in u
Cubic
cubic in u
Quintic
quintic in u
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.