SectionSurfaceBuilderExSpineStartFlowType Enumeration

NXOpen.Features.SectionSurfaceBuilderEx.SpineStartFlowType is an alias for NXOpen.Features.SectionSurfaceBuilderExSpineStartFlowType

class NXOpen.Features.SectionSurfaceBuilderExSpineStartFlowType

Bases: object

Spine Start Flow type.

Enum Members

Enum Member Enum Member Description
NotSpecified
flow direction not specified
Perpendicular
flow direction perpendicular to the guide
IsoLineU
flow direction follows iso u of the start surface
IsoLineV
flow direction follows iso v of the start surface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.