SectionSurfaceBuilderExSpineEndFlowType Enumeration¶
NXOpen.Features.SectionSurfaceBuilderEx.SpineEndFlowType is an alias for NXOpen.Features.SectionSurfaceBuilderExSpineEndFlowType
-
class
NXOpen.Features.
SectionSurfaceBuilderExSpineEndFlowType
¶ Bases:
object
Spine End Flow type.
Enum Members
Enum Member Enum Member Description NotSpecified flow direction not specifiedPerpendicular flow direction perpendicular to the guideIsoLineU flow direction follows iso u of the start surfaceIsoLineV flow direction follows iso v of the start surface-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-