SectionSurfaceBuilderExSpine Enumeration

NXOpen.Features.SectionSurfaceBuilderEx.Spine is an alias for NXOpen.Features.SectionSurfaceBuilderExSpine

class NXOpen.Features.SectionSurfaceBuilderExSpine

Bases: object

Spine type.

Enum Members

Enum Member Enum Member Description
ByVector
spine by vector
ByCurve
spine by curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.