SectionSurfaceBuilderExSlopeControlType Enumeration

NXOpen.Features.SectionSurfaceBuilderEx.SlopeControlType is an alias for NXOpen.Features.SectionSurfaceBuilderExSlopeControlType

class NXOpen.Features.SectionSurfaceBuilderExSlopeControlType

Bases: object

Slope Control type.

Enum Members

Enum Member Enum Member Description
ByApex
slope control by apex
ByCurves
slope control by curves
ByFaces
slope control by faces
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.