SectionSurfaceBuilderExCubicType Enumeration

NXOpen.Features.SectionSurfaceBuilderEx.CubicType is an alias for NXOpen.Features.SectionSurfaceBuilderExCubicType

class NXOpen.Features.SectionSurfaceBuilderExCubicType

Bases: object

This enum represents the current modes of cubic type section surfaces.

Enum Members

Enum Member Enum Member Description
TwoSlopes
Two Slopes mode
FilletBridge
Fillet Bridge mode
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.