SectionCurveBuilderSpacingType Enumeration

NXOpen.Features.SectionCurveBuilder.SpacingType is an alias for NXOpen.Features.SectionCurveBuilderSpacingType

class NXOpen.Features.SectionCurveBuilderSpacingType

Bases: object

Represents spacing type.

Enum Members

Enum Member Enum Member Description
EqualArcLength
Equal arclength spacing
EqualParameterSpacing
Equal parameter spacing
GeometricProgressionSpacing
Geometric progression spacing
ChordalToleranceSpacing
Chordal tolerance spacing
IncrementalArclengthSpacing
Incremental arclength spacing
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.