RibBuilderRibThicknessOffsetOptions Enumeration

NXOpen.Features.RibBuilder.RibThicknessOffsetOptions is an alias for NXOpen.Features.RibBuilderRibThicknessOffsetOptions

class NXOpen.Features.RibBuilderRibThicknessOffsetOptions

Bases: object

These represent the options for Rib Walls Offset

Enum Members

Enum Member Enum Member Description
Symmetric
Symmetric Offset
Asymmetric
Asymmetric Offset
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.